"Now the operator is inspecting parts coming out of the machine and programming the robot instead of operating the machine."
“I can spend more time programming machines since I don’t have to load them. Plus, there’s more consistency in the loading. It’s taken away some of the human error.”
"What Robotiq’s grippers have to offer is a step beyond any of the competitors."
“We went from making about 1,000, 1,500, or 2,000 parts at a time, to about 45,000–50,000 of these parts.”
“The robot handles any of our 300 different parts with a single parametric program. When we make a change, we only have to do it once.”
“The big advantage of the force torque sensor is that you can record complex movements with the path-recording function.”
“The whole integration went very smoothly. Half our staff is over 40 years old, and everyone found it easy to learn to work with Robotiq and Universal Robots.”
“Factories don’t buy a robot to replace people, they buy it because they cannot find people. I’ve never seen someone in Romania lose his job to a robot.”
“In getting the Robotiq gripper to work with the UR10, I just had to drag blocks of information onto the robot’s screen, link up the different blocks and it basically runs itself.”
“Whether I’m in the shop or not, Insights signals any stop immediately. I then put the robot back into production faster. Minimum downtime means higher productivity.”
“It freed up skilled workers to do value-added activity as opposed to loading-unloading the machine.”
“The robot not only relieves our machinists from moving parts in and out of the machine, it gives them time to work on their new motivating challenge, which is to program the robot’s waypoints with the production setup in mind.”
“The repeatability and the consistency of what’s going on in the machine is a huge plus for us. We make high-end quality products, it is very important to deliver the same standard in every production.”
“The integration of collaborative robots was so much easier than the previous ones we had. We do not need much sensors around the equipment. It is really efficient. I saw immediately the advantages, easy integration, zero maintenance, higher productivity. Our changeover time is twice faster now.”