“The cobots are fast, but I can keep up—and it’s great how much we’ve increased our numbers.”
“We went from making about 1,000, 1,500, or 2,000 parts at a time, to about 45,000–50,000 of these parts.”
"Now the operator is inspecting parts coming out of the machine and programming the robot instead of operating the machine."
“I can spend more time programming machines since I don’t have to load them. Plus, there’s more consistency in the loading. It’s taken away some of the human error.”
“The big advantage of the force torque sensor is that you can record complex movements with the path-recording function.”
“Whether I’m in the shop or not, Insights signals any stop immediately. I then put the robot back into production faster. Minimum downtime means higher productivity.”
“The integration of collaborative robots was so much easier than the previous ones we had. We do not need much sensors around the equipment. It is really efficient. I saw immediately the advantages, easy integration, zero maintenance, higher productivity. Our changeover time is twice faster now.”