-1.jpeg?width=2000&name=2F85-Wrist-Camera-Machine-Tending-Walt-Machine-58%20(1)-1.jpeg) 
	Case Studies
Walt Machine
The evolution of a machine shop
2500%
Production increase
3
CNCs
3
CNCs
About Walt Machine
Walt Machine makes precision aluminum parts for optical assemblies—their specialty—and offers other manufacturing services. 
                    
                    Step 1 - Box dimensions, weight and orientation
 
                    
                    Step 1 - Box dimensions, weight and orientation
 
                    
                    Step 1 - Box dimensions, weight and orientation
Leveraging cobots to deliver 6000 camera housings in 2 months’ time, with only one CNC machine.
          We went from making about 1,000, 1,500, or 2,000 parts at a time, to about 45,000-50,000 of these parts.
 
                Tommy Caughey
                President, Walt Machine
                Overcoming Challenges: Our Solutions
The Problem
Since our last case study with WALT Machine Inc., they have seen a huge increase in demand, but hiring new employees hasn’t gotten any easier. Tommy Caughey, president of WALT Machine Inc. has already succeeded with automating a first CNC machine. He is now looking to scale its production and automation capabilities to meet growing customer needs.The Solution
Caughey already had part of the answer with his first application. He started small instead of trying to automate everything at once. It worked: his Robotiq 2F-140 Gripper, installed on a ceiling-mounted Universal Robot UR10, is tending three different machines. He’s now installing a Robotiq CNC Machine Tending Kit on a new UR and automating a second application. 
                        
                      
                    
                    
                  
                    The Results
                Increased productivity
Robotiq Machine Tending Solution helped increase productivity and consistency:
- Productivity: The results speak for themselves. Whereas one robot doubled daily production, two robots have let them increase production by 2,500%.
- Dealing with a small footprint: As Walt Machine was dealing with a very small footprint, the robots were installed on a rail to the ceiling of the facility.
The Robotiq solution
Walt Machine installed a Robotiq 2-Finger 140 Gripper on a UR10 cobot to tend CNC machines around the clock, which doubled daily production.
          .jpg) 
               
                        
                      
                    
                    
                  
                    Applications
                Machine Tending
Walt Machine initially installed a Robotiq Wrist Camera and 2-Finger 140 Gripper on a UR10 cobot to tend CNC machines around the clock, which doubled daily production. Since then, they’ve added two more robots and scaled up from making 2,000 parts to 50,000 parts.