Vincent and Hugo from Usinatech content with Robotiq Machine Tending Solution

Case Studies

Machine tending automation for automotive parts manufacturers | Usinatech

The art of implementing cobots on a busy production floor

Robotiq logotype as a home icon • Resource center • Case Studies • Usinatech

3 CNCs

The number of stations an operator can manage simultaneously (instead of just one).

6 Robotiq Machine Tending Kits

To help face a labor shortage and increase operator productivity

50%

Lower implementation cost than industrial robots

About Usinatech

Located in Melbourne, Quebec, Usinatech has been making critical drivetrain and transmission components, like gears and shafts, since 1986. They employ 300 people in   Canada and 50 more in Mexico. Usinatech has been automating its production cells for many years. However,  the growing labor shortage and the need to become even more competitive in the market have forced   Usinatech to accelerate its shift to automation. 

Number of Employees

350

Products

Machine Tending Solution

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

Usinatech: The art of implementing cobots on a busy production floor
What Robotiq’s grippers have to offer is a step beyond any of the competitors.
Vincent Usinatech
Vincent Roussy
Manufacturing Engineering Manager

Overcoming Challenges: Our Solutions

The Problem

Since 2017, the growing labor shortage and the need to become even more competitive in the market have created a lot of pressure on the manufacturing floor. According to Usinatech, automation was the way to go!

The Solution

Usinatech accelerated its shift to automation. Patrick Coté and Vincent Roussy are glad to say this shift has resulted in significant productivity gains, lower operating costs, and a lower employee turnover rate, which has stabilized all aspects of production and distribution.
Cobot Machine Tending at Usinatech Facility
The Results

Effective ROI.

Robotiq’s Machine Tending Solution brought benefits on many levels:

  • User-friendly: Usinatech integrated the first three cobots by themselves. Once tested and standardized, the process became so simple and efficient that cobot implementations are now an internship project for college students.
  • ROI: The total project cost for implementing a cobot at Usinatech is at least 50% lower than for an industrial robot.

The Robotiq solution

Usinatech’s decision to automate cells using both Robotiq’s collaborative robots and insights from lean robotics has led to a faster ROI
Vincent+Hugo 2
Machine_Tending_Solution_3D_Cad
Applications

Machine Tending

Usinatech’s decision to automate cells using both the Robotiq Machine Tending Solution and insights from lean robotics has led to a faster ROI.

Find out how we can help achieve results like these for you