Case Studies
Palletizing automation for industrial equipment manufacturers | Korea Filter Engineering
Efficiency Without Compromise: Korea Filter Engineering Protects Workers with Robotiq PE20
4 tonnes
Total packaging weight
20 SKUs
Boxes handled
2130 mm
Max pallet height
About Korea Filter Engineering
Korea Filter Engineering, founded in 1996, specializes in industrial filters used in electrical discharge machining (EDM). The company focuses on precision and quality, producing filters for the global industrial market. With a lean team of 15 employees, the company relies on skilled operators to maintain efficiency and quality.
Step 1 - Box dimensions, weight and orientation
Step 1 - Box dimensions, weight and orientation
Step 1 - Box dimensions, weight and orientation
The Problem
Korea Filter Engineering processes heavy industrial filter boxes weighing 10–20 kg, with employees manually lifting around 4 tons of material per day. This caused frequent back, shoulder, and muscle strain, especially given an aging workforce, leading to higher injury risk, absenteeism, and reduced productivity. Although they tried different lifting methods, operations always returned to fully manual palletizing, further decreasing efficiency, lowering employee morale, and even causing delivery delays.
The Solution
To address these challenges, Korea Filter Engineering implemented the Robotiq PE20 Palletizing Solution with a UR20 cobot. The compact, collaborative robot works safely alongside staff without protective enclosures, integrates smoothly with the conveyor system, and handles repetitive palletizing tasks efficiently. Its intuitive interface allows any operator to learn basic operations quickly, enabling the company to increase productivity while protecting workers from physical strain.
Convincing wins.
Robotiq’s palletizing cobot brought measurable advantages at every level:
- Higher Productivity: Production speed increased by 30%, raising daily output from 200 to 250 boxes.
- Reduced Physical Strain: Injury-related absences and worker fatigue were both reduced by roughly 50%, improving overall workplace well-being.
- Better Workforce Allocation: One full-time employee was reassigned to higher-value tasks, increasing operational efficiency.
- Fast Return on Investment: With significant gains in safety and productivity, the expected ROI is under two years.
- Improved Workplace Safety: Since installation, there have been zero workplace accidents, reinforcing a safer, more reliable palletizing process.
Voices From the Shop Floor
Leadership: Driving Operational Excellence
Management highlights that the PE20 has brought more predictability to daily operations. With safer workflows and fewer disruptions, the team can focus on long-term improvement instead of short-term firefighting.
On the Floor: Empowering Daily Work
On the production floor, employees say the biggest change is how work feels—lighter, smoother, and less physically demanding. Operators adapted quickly thanks to the intuitive interface, and collaboration between shifts has naturally improved.
Palletizing
The PE20 solution has transformed Korea Filter Engineering’s operations: increasing efficiency, eliminating physically demanding manual stacking, and enabling safe, continuous workflow while handling a diverse range of filter boxes.