Robotiq enables Physical AI
Robotiq enables Physical AI by giving robots the sense of touch and control they need to learn and act in the real world.
The Physical Foundation for AI
Robotiq is a recognized leader in adaptive grippers and accessories, with over 30,000 units deployed worldwide.
Our products work together to provide the core physical interaction and sensing capabilities required for multimodal learning, robotic manipulation, and Physical AI foundation model training.
By combining proven, robust hardware with multiple sensing modalities, Robotiq addresses two of the main challenges in physical AI today: data and reliable deployment.
Are you innovating fast in Physical AI?
Perception to Action
Robotiq products provide the physical interaction and feedback layer that allows AI systems to act in the real world.
Adaptive grippers mechanically conform to object variability, reducing the need for precise grasp planning, while force, torque, and tactile sensing deliver real-time physical signals for closed-loop control and learning.
Integrated with modern robotics and AI models, Robotiq hardware turns AI decisions into robust, data-rich physical actions.
Repositories
Community & Third-Party
Customer Applications
2FC Physical AI Gripper
A production-ready adaptive gripper with tactile sensing and embedded intelligence, helping robots learn from physical interaction and act reliably on what they learn, from the lab to production.
Embedded intelligence: With compute built into the gripper, the 2FC runs grasp skills locally and in real time.
Contact-rich data: More modalities, timestamped and synchronized with automatic labeling.
Durability and reliability: Train and deploy on the same hardware.
Adaptive Grippers
Adaptive grippers form the foundation of Physical AI manipulation. Robotiq’s 2F-85, 2F-140 and Hand-E grippers provide a simple, robust way to interact with a wide range of real-world objects.
High uptime: Reliable manipulation in unpredictable environments featuring a patented encompassing grip.
Consistent at scale: Proven, repeatable, and robust hardware with 23 000+ grippers deployed.
Flexible integration: Designed for modern AI pipelines with standard communication protocols.
Tactile Sensor Fingertips
The TSF-85 provides rich multimodal data
for foundation model training, enables better grasp decisions and stability, improves generalization across objects and contact geometry for a consistent grip.
Pressure for contact awareness with 28 taxels.
Vibration for slip detection at 1000 Hz.
Proprioception for accurate finger orientation with IMU sensing.
Force Torque Sensor
The FT-300-S is a 6-DOF force-torque sensor that gives Physical AI systems precise, high-resolution contact awareness for compliant, contact-rich manipulation.
By accurately detecting and measuring interaction forces, it enables robots to regulate contact, adapt to variability, and recover from uncertainty in real-world tasks, reducing tuning effort, simplifying programming, and accelerating the transition from simulation to reliable deployment.
Contact Core
Contact Core is Robotiq's software layer for Physical AI. It gives model builders the simulation assets in NVIDIA Isaac Sim, control packages in ROS2, and synchronized contact-rich data interfaces they need to train manipulation models on Robotiq components and deploy them on real robots.

Frequently Asked Questions
What is Physical AI?
Physical AI, also called embodied AI, is AI paired with a robot that perceives, decides and acts in the real world. It lets machines interpret their environment, make decisions and carry out tasks autonomously — reaching, grasping, manipulating and interacting with objects. Because those actions depend on real physical contact, hardware and sensing play a central role in making Physical AI work.
Why is data the main bottleneck in Physical AI?
Physical AI needs far more real-world interaction data than exists today. Unlike text, that data cannot be scraped — it has to be generated one trajectory at a time, on physical robots. The rate at which reliable, contact-rich data is collected now limits how fast generalist robot policies improve.
Why isn't vision enough for robot manipulation?
Vision shows what an object looks like, not what it feels like to grasp. Forces, torques, pressure and vibration only register on contact — and those signals decide whether a grasp holds, an insertion succeeds, or a fragile part survives. The strongest manipulation models combine vision with force-torque and tactile data at the end-effector, which is why instrumented grippers and wrist sensors are becoming standard in Physical AI pipelines.
How does Robotiq support Physical AI foundation model training?
Robotiq provides the physical interaction and feedback layer Physical AI models need. Adaptive grippers, the FT-300-S force-torque sensor and the TSF-85 tactile fingertips generate synchronised, multimodal data — force, torque, pressure, vibration and proprioception — for policy learning. Standardised ROS packages and NVIDIA Isaac Sim assets bridge simulation and reality, while 17 years of industrial-grade hardware design makes the resulting data reliable at scale.
Which Robotiq products anchor a Physical AI stack?
Three product families cover the perception-to-action loop. Adaptive grippers: 2F-85 (85 mm stroke, 5 kg payload), 2F-140 (140 mm, 2.5 kg), and Hand-E (50 mm, 7 kg). Tactile fingertips: the TSF-85, which swaps onto the 2F-85 and 2F-140. Force-torque: the FT-300-S, a 6-DOF sensor with ±300 N range and 500% overload capacity. All integrate with ROS, ROS 2 and NVIDIA Isaac Sim.
How reliable is Robotiq hardware?
Robotiq grippers are built for industrial duty cycles. The 2F-85 and 2F-140 carry a 2-million-cycle warranty at IP40, and the Hand-E a 5-million-cycle warranty at IP67. In practice, most units run well beyond those numbers. The TSF-85 is rated for over 1.5 million cycles. That durability matters in Physical AI because every hour a robot stays running is an hour it can collect training data.
What does the TSF-85 tactile sensor measure?
The TSF-85 captures three signals at the fingertip. Pressure is read across a 28-taxel capacitive array for contact shape and intensity. Vibration is sampled at 1000 Hz to detect slip. An IMU tracks fingertip orientation. It swaps onto the 2F-85 and 2F-140 without reducing gripper stroke.