Robotiq Palletizing Solutions

Simple to deploy. Proven to perform. Built to scale.

 

Automation made easy — really.

Manual palletizing is hard to staff and harder to scale. Our solution changes that.

The Robotiq Palletizing Solution is fast to set up, easy to use, and ready to scale with your business.

It’s everything you need, nothing you don’t.

Presentation

PAL-Beforeafter-PE20-wcopy

Robotiq Palletizing Solution - small steps, big impact

Your end-of-line is the final stop before delivery to your customers. It's also one of the most manual and labor-intensive.

Robotiq helps you automate it—without complexity, long timelines, or rigid systems.

Empower your people. Boost your factory productivity. Enhance your adaptability.

Safer work

Remove repetitive tasks and reduce strain.

Smarter deployment and faster ROI

Easy to set up. Easy to use. No robotics experience needed.

Predictable payback in 1-2 years.

More adaptability

Handle new SKUs, pallet patterns, and setups with ease.

What's included in the Robotiq Palletizing Solution?

blog.robotiq.comhubfsHack AG palletizing factory

Fast setup with standard modules


The Robotiq Palletizing Solution is a standard, pre-engineered system that’s ready to work. It’s compact, robust, and built to keep up with your production.

 

CoPilot palletizing software that works like your best operator

  • Visual setup requires no code
  • Auto-optimizes trajectories 
  • Handles obstacles and tight layouts 
  • Allows for cloning and reusing recipes
  • Built-in Force & Torque sensor for stacking precision

 

A complete, proven system—delivered turnkey.

When you choose Robtoiq, you're not just getting a palletizer—you’re getting end-to-end support, from initial design to full-scale operation:

  • Turnkey setup in 3 days
  • Training included
  • Backed by Lean Robotics methodology
  • Delivered by certified Expert Partners or by Robotiq Installation Services

How we make it work for you

Come see it in action

Prefer a hands-on look? See a map of local Expert Partners for a live demo—bring your own products and see it in action.

 

How we get you from idea to operation

Our Application Experts will guide you through the deployment process. 

  1. Design: We gather your information and simulate a fit
  2. Integrate: Pre-tested, optional FAT (Factory Acceptance Testing)
  3. Operate: Local install and training in three days
Deanan-footprint (1)

Small footprint

Installs in 3 days. Fits your space. Scales with you.

No need to reconfigure your line or halt production.

Robotiq’s compact system fits your layout now and grows with it later.

How much does it cost?

How much does it cost?

The exact cost depends on your factory’s setup, but the payoff is clear—most factories see ROI in 1–2 years through labor savings, higher output, and lower hiring costs.


Want real numbers for your operation? Try our ROI calculator to crunch the numbers.

Ready to move forward? 

Who's using it?

Robotiq_Glenhaven-15-1
Real results from real factories

"So really it's a very quick, fast, simple solution, and it's one that can be rolled out at pace across multiple lines within a factory."

- Ken Maguire
Managing Director, Glenhaven Foods

09_2024_WE_CaseStory_Raumland 16-1
Real results from real factories

"The cobot perfectly reflects what we need. It is a flexible machine, compact, quick to set up, and, ultimately, affordable. We were able to automate a task that was extremely tedious. No one complains about back pain anymore. At least not from palletizing."

- Sebastian Raumland
Managing Director, Raumland GmbH

cascade-coffee
Real results from real factories

"The ROI was a slam dunk from the beginning, from how much labor it saved. The installation process was the smoothest install of any piece of equipment I have had to experience in 28 years."

- Greg Thayer
Vice-President, Cascade Coffee

Hack AG
Real results from real factories

"The key result for our production process is that we are now further flexible in our processes and product planning, and we decreased the hard work of our employees."

- Simon Gunnemann
Managing director central production, Hack AG



FAQ

What's a cobot?
A cobot (collaborative robot) works safely alongside people, boosting productivity without barriers. Built with advanced sensors and smart programming, it adapts to human interaction—no cages, no complexity.
What robot do you use?
We use industry-leading Universal Robots in all of our palletizing solutions for their reliability, ease of use, and seamless integration. They’re built for flexibility, safety, and fast deployment—so you get up and running in no time.
How safe is it?

Cobot palletizing doesn’t just meet safety standards—it improves workplace safety. Manual palletizing leads to fatigue and injury from repetitive lifting and awkward postures. Automating with cobots eliminates these risks while built-in safety features like force detection, collision prevention, and controlled speeds keep operations secure.
For more information, download our ergonomics ebook

What if it breaks?

We’ve designed our solutions for reliability—standardized hardware, smart software, and fast installation keep downtime to a minimum. If an issue comes up, troubleshooting is simple, and our local support network gets you back up and running fast. Plus, with decentralized palletizing, there’s no single point of failure, so your lines keep moving.

How is it different from other solutions?

Unlike centralized solutions or industrial palletizers that require extensive conveyor rerouting and reduce operational flexibility, our cobot palletizing solutions keep your lines flexible and resilient. Designed for Lean Robotics, they integrate seamlessly into existing layouts—no extensive modifications needed.

Our advanced control algorithms and tooling deliver higher throughput than other cobot solutions. Unlike rigid "in-a-box" systems, Robotiq’s palletizer scales with you, integrating additional automation as your needs evolve.
And while custom-engineered palletizers require long design cycles, ours offers short lead times and intuitive software, making it easy to add new products or pallet patterns. For more information see our Automated Palletizing Buyer’s Guide.

Where can I see it in action?

Our global network of Expert Partners is available to show you a demo. You can even test a Robotiq Palletizing Solution with your own products if you wish! Book a demo with an Expert Partner near you.

The Robotiq team also travels regularly to trade shows to give live demos of the Robotiq Palletizing Solution. Check out our events page to see if we'll be in your area soon!

What is Lean Robotics?
Lean Robotics is a methodology for simplifying robotic cell deployments. It is a systematic way to complete the robotic cell deployment cycle, from design to integration and operation.
The Lean Robotics book by Robotiq CEO Samuel Bouchard is the result of a decade of the company’s experience helping thousands of manufacturers overcome production challenges using robots.

Ready when you are!

Fast lead times. 2-year warranty. 98% satisfaction with customer support.
Start small. Scale smart. Let’s get to work.