Nutriset-palletizing-2

Case Studies

Nutriset

Fueling innovation: Nutriset's automated solution for global nutrition

6 mo

Estimated return on investiment

400

Cartons packed daily

2.20

Meter high pallets

About Nutriset

Nutriset, a leading French company headquartered in Normandy, specializes in the research, development, production, and worldwide distribution of specialized nutritional foods designed to treat and prevent various forms of malnutrition. In response to the challenges posed by the post-Covid era, Nutriset embarked on an automation project to fully automate its production line.

Industry

Food & beverage

Number of Employees

280

Products

Palletizing Solution

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

701daf01b9d82dc07055eb4e6f9ba6ee79eb991c609c58a5ceccee00975ee0e3 1

Step 1 - Box dimensions, weight and orientation

Nutriset: Reduction in musculoskeletal disorders (MSD) associated with palletizing tasks
We had a two-day production stop while we installed the robot and made the first pallets. So it's extremely simple, extremely facilitated by the fact that it arrives turnkey.
sylvain-clausse
Sylvain Clausse
EIA Coordinator, Nutriset

The Problem

Manual post-Covid palletizing posed major challenges for Nutriset. Keen to fully automate its production line, Nutriset faced obstacles such as inconclusive tests due to high payload requirements, limited space, low ceilings, heavy and oversized cartons, as well as pre-cuts on the cartons, which made the process even more complex.

The Solution

While initial trials were inconclusive, the breakthrough came with Robotiq's Palletizing Solution paired with the UR20, which offered the necessary collaborative solution without the need for safety cages making it 100% collaborative. Leveraging Robotiq's expertise and team, Nutriset found the ideal automation configuration to efficiently streamline its palletizing process.

nutriset pal
The Results

Convincing wins.

Robotiq’s palletizing cobot brought benefits on many levels:

  • Reduced musculoskeletal disorders (MSDs): Significant reduction in repetitive strain injuries associated with palletizing tasks, resulting in a healthier workforce.
  • Increased productivity: Improved operational flexibility and reduced downtime have led to substantial productivity gains, streamlining all processes.
  • Rapid return on investment: The rapid integration of the automated solution resulted in an estimated return on investment of 6 months.

The Robotiq solution

The Robotiq Palletizing Solution improved Nutriset's productivity thanks to reduced downtime and enhanced operational flexibility.
nutriset pal solution
Palletizing Solution - PE
Applications

Palletizing

The Robotiq Palletizing solution transformed Napco’s operations: not only did it lead to a 15% increase in production, but it also reduced the risk of injuries and allowed the company to reallocate eight workers per day to more specialized tasks. 

Find out how we can help achieve results like these for you