CASE STUDIES
Palletizing automation for champagne houses and wineries | Champagne Gosset
How Champagne Gosset automated case palletizing with a collaborative palletizer
Key results
5 weeks
Full deployment after a simulation validated with Sysaxes, without reorganizing the end of the line.
11.5 kg
Repetitive lifting of cases weighing up to 11.5 kg is eliminated, reducing MSD exposure and the mental load of the job.
A few hours
All operators need to create and adjust palletizing recipes themselves, from standard cases to magnums.
Company overview
Step 1 - Box dimensions, weight and orientation
Step 1 - Box dimensions, weight and orientation
Step 1 - Box dimensions, weight and orientation
About Champagne Gosset
Founded in Aÿ in 1584, Gosset is the oldest wine house in Champagne. Family-owned and independent, it is the only Champagne house that is both a member of L’Excellence Française and certified as an “Entreprise du Patrimoine Vivant” (Living Heritage Company).
Like many houses, Gosset relied on manual palletizing at the end of its bottling line. To make the job less strenuous without giving up its flexible organization, the house turned to collaborative palletizing.
The challenge
Before automation, palletizing was the last manual step on the bottling line. An operator lifted the cases and stacked them on pallets following a production sheet.
This manual process created several challenges:
- Repetitive heavy lifting: cases up to 11.5 kg and exposure to MSDs
- A heavy mental load in a strenuous job
- A bottleneck at the end of the line
- A constrained workshop: limited space, low ceiling and pallets up to 1.85 m
- Varied formats, from standard cases to magnums
Gosset also had specific requirements: some gift boxes must be placed on edge. Above all, the house wanted to keep its way of working, which had already ruled out several solutions.
The solution
To automate its end of line, Champagne Gosset chose Robotiq’s PE20 palletizing solution, with a UR20 cobot from Universal Robots and a Robotiq vacuum gripper.
The palletizing cell includes:
- Robotiq Lean Palletizing PE20
- UR20 cobot (1,750 mm reach, 20 kg payload)
- Robotiq vacuum gripper [model to be confirmed]
- Robotiq palletizing software
- Two pallets handled simultaneously
- Contact detection for fenceless operation
The configuration was validated upfront with a simulation by Sysaxes, official distributor of Universal Robots and Robotiq. The system was deployed in five weeks and builds 1.85 m pallets under a low ceiling.
Why Champagne Gosset chose Robotiq
A small footprint
Space and ceiling height were limited. The PE20 fit into the existing workshop while building 1.85 m pallets.
A solution that adapts to the house’s methods
Robotiq software handles multiple recipes, including magnums and gift boxes placed on edge, without changing how operators work.
Up and running in a few hours
With support from UR Academy, a few hours were enough. Operators create and launch recipes themselves, with no programming skills.
A cobot the team has adopted
The cobot works without fencing alongside operators, who focus on quality control and finishing. The team has even given it a name.
The Robotiq solution
Frequently asked questions
Is Robotiq specialized in palletizing for champagne houses and wineries?
Yes. Robotiq has deployed palletizing solutions in wineries, champagne houses and distilleries. Its collaborative palletizers handle heavy cases and fit into tight spaces.
Can a collaborative palletizer handle heavy champagne cases?
Yes. At Champagne Gosset, the PE20 handles cases weighing up to 11.5 kg with a Robotiq vacuum gripper. Robotiq Lean Palletizing handles cases up to 32 kg and up to 13 picks per minute.
How do you palletize different champagne case formats?
The palletizing pattern takes into account the bottle format, the case dimensions and orientation, and the target pallet height. At Gosset, the PE20 handles standard cases, magnums and gift boxes placed on edge.
Can a palletizer fit into a small workshop?
Yes. Collaborative palletizers have a much smaller footprint than traditional systems. At Gosset, the PE20 builds 1.85 m pallets under a low ceiling, without a safety cage.
Can operators adjust the palletizer themselves?
Yes. Robotiq software lets operators create and launch recipes by entering case dimensions, weight and palletizing pattern, with no advanced programming training.
Is your end of line ready for automation?
If your operation:
- palletizes manually with ergonomic risks
- handles a variety of packaging formats
- has limited production space
A collaborative palletizer can be up and running in a few weeks.