Home
Documentation
Learning Center
DoF
Tools
Events
Contact us Careers Support

The art of implementing cobots on a busy production floor

Problem

Since 2017, the growing labor shortage and the need to become even more competitive in the market have created a lot of pressure on the manufacturing floor. According to Usinatech, automation was the way to go!

Solution

Usinatech accelerated its shift to automation. Patrick Coté and Vincent Roussy are glad to say this shift has resulted in significant productivity gains, lower operating costs, and a lower employee turnover rate, which in turn has stabilized all aspects of production and distribution.

Don’t have time to go through the full case study?
Get the free PDF for later

Products they use

Applications

Machine Tending

Pick & Place

By the numbers
3
CNC machines
The number of stations Hugo can now manage simultaneously (instead of just one).
6
Robotiq CNC Machine Tending Kits
to help face a labor shortage and increase operator productivity
50%
lower implementation cost
than industrial robots

Got a challenge for us?

Let's work together