About
Contact Us
Careers
Support
En
Why Automation?
Products
Solutions
Resources
Start Now
Home
Why Automation?
Case Studies
Applications
Management Benefits
Engineering Benefits
Lean Robotics Methodology
Products
Grippers
2F-85 and 2F-140 Adaptive Grippers
Hand-E
3-Finger Gripper
Vacuum Grippers
Sensing and Vision
Wrist Camera
Force Copilot
FT 300-S Force Torque Sensor
Finishing Copilot
Production Monitoring
Insights
Application Kits
Sanding Kit
na
Product Configurator
Surface Finishing Kit
Solutions
Palletizing Solution
Screwdriving Solution
Machine Tending Solution
Solutions
Palletizing Solution
Machine Tending Solution
Screwdriving Solution
Resources
Documentation
Catalog
Case Studies
eBooks
Photos & Videos
Blog
Podcasts
Getting Started
Learning Center
eLearning
On-Site Trainings
DoF
Tools
ROI Calculator
Events
Upcoming Events
Start Now
Get a Quote
Create Your Own Blueprint
Contact Your Local Distributor
About
Who We Are
About the Team
Media Coverage
Contact us
Careers
Support
En
All
Resource Center
Blog
Support
DoF
Home
Resources
Application Packages
Application Packages
Find, Measure and Locate Center
The Find, Measure and Locate Center application package allows you to perform search instructions in the X, Y or Z axis of the tool to locate parts. The high sensitivity of the Force Torque Sensor all…
Path Height Control
The goal of this package is to record a path and play it back relative to its start position. Using the path recording feature of our Force Torque Sensor and some programming tools, you will be able t…
Measuring Insertion Force
The goal of this application package is to measure the force applied to the robot during a robot motion. It could be used in assembly tasks or in testing applications to measure the maximum force in a…
Manage Stacks
This application package allows you to manage objects in stacked trays using the Wrist Camera. It uses an advanced function that enables the use of the same snapshot position at different heights.
Stacking/Unstacking Parts
This application package allows you to stack or unstack parts using a Robotiq Force Torque Sensor. It uses the force feedback received from the sensor to detect when it touches a surface.
Data Logging from UR Program to External PC
This package allows you to log variables in an external PC; results like maximum forces, robot positions, number of cycles in a standard CSV file.
Detecting Thin Objects
With the help of the included fingertips (CAD file) this simple application package allows you to detect the presence of objects with a thickness as thin as 1.2 mm.
Placing a Part With Three Reference Points
This application package provides a program allowing to place a part with good positional repeatability by using the force data provided by the FT 300 Force Torque Sensor to find three reference point…
Measuring an Object
This application package uses the Gripper's opening position detection built-in is feature to determine the dimension of an object between the Gripper fingertips.
Sensor to CSV File Streaming Data
Using the Ethernet port on the UR controller, it is possible to stream data from the FT 150 or FT 300 on a computer using the StreamToCsv software.
Increasing Field of View
The main objective of this application package is to provide a program allowing you to increase the Wrist Camera’s field of view.
Questions? Our team is here to help
Contact Robotiq support